PartOperationImportBuilderExistingPartAction Enumeration

NXOpen.PDM.PartOperationImportBuilder.ExistingPartAction is an alias for NXOpen.PDM.PartOperationImportBuilderExistingPartAction

class NXOpen.PDM.PartOperationImportBuilderExistingPartAction

Bases: object

This enum is used to specify the default action for import.

Enum Members

Enum Member Enum Member Description
Overwrite
UseExisting
NewRevision
Default
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.