PartOperationImportBuilderConversionRule Enumeration

NXOpen.PDM.PartOperationImportBuilder.ConversionRule is an alias for NXOpen.PDM.PartOperationImportBuilderConversionRule

class NXOpen.PDM.PartOperationImportBuilderConversionRule

Bases: object

This enum is used to specify the conversion rule for NXOpen.PDM.PartOperationImportBuilderNumberingSourceOption.OSFilename.

Enum Members

Enum Member Enum Member Description
AsID
AsIDandRevision
WithPrefix
WithSuffix
WithReplaceString
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.