PartOperationCreateBuilderOperationSubType Enumeration¶
NXOpen.PDM.PartOperationCreateBuilder.OperationSubType is an alias for NXOpen.PDM.PartOperationCreateBuilderOperationSubType
-
class
NXOpen.PDM.
PartOperationCreateBuilderOperationSubType
¶ Bases:
object
Represents an operation sub type for creating a part
Enum Members
Enum Member Enum Member Description FromTemplate Create New Part from template SelectTemplate Populate Part already created in Teamcenter Rename Rename Existing Part CreateSpecification Create Specification and not a Part -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-