ErrorMessageHandler Class¶
-
class
NXOpen.PDM.
ErrorMessageHandler
¶ Bases:
NXOpen.TransientObject
Represents the class that contains ErrorObjects and Failed Logical Objects.
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the instance. |
GetErrorList | Returns ERROR_LIST_s |
GetErrorMessages | Returns Error Messages |
GetWarningMessages | Returns Warning Messages |
Method Detail¶
Dispose¶
-
ErrorMessageHandler.
Dispose
¶ Free resources associated with the instance.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetErrorList¶
-
ErrorMessageHandler.
GetErrorList
¶ Returns ERROR_LIST_s
Signature
GetErrorList()
Returns: Return type: NXOpen.ErrorList
New in version NX11.0.0.
License requirements: None.