Methods¶
Method | Description |
---|---|
Dispose | Frees the object from memory. |
GetCommandName | Returns the command name |
GetSelectedUids | Returns the unique identifier of the uids in PDM |
RegisterCustomWebAppInvokedCallback | Registers the add_custom_web_app_menu_callback callback method with the webApp menu handler object. |
Method Detail¶
Dispose¶
-
CustomWebAppMenuHandler.
Dispose
¶ Frees the object from memory.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX11.0.0.
License requirements: None.
GetCommandName¶
-
CustomWebAppMenuHandler.
GetCommandName
¶ Returns the command name
Signature
GetCommandName()
Returns: the command name Return type: str New in version NX11.0.0.
License requirements: None.
GetSelectedUids¶
-
CustomWebAppMenuHandler.
GetSelectedUids
¶ Returns the unique identifier of the uids in PDM
Signature
GetSelectedUids()
Returns: Selected uids Return type: list of str New in version NX11.0.0.
License requirements: None.
RegisterCustomWebAppInvokedCallback¶
-
CustomWebAppMenuHandler.
RegisterCustomWebAppInvokedCallback
¶ Registers the add_custom_web_app_menu_callback callback method with the webApp menu handler object.
Signature
RegisterCustomWebAppInvokedCallback(webappCb)
Parameters: webappCb (CallableObject) – New in version NX11.0.0.
License requirements: None.