CaeCloneManagerCloneOption Enumeration

NXOpen.PDM.CaeCloneManager.CloneOption is an alias for NXOpen.PDM.CaeCloneManagerCloneOption

class NXOpen.PDM.CaeCloneManagerCloneOption

Bases: object

Option for creation of part builder for CAE Clone

Enum Members

Enum Member Enum Member Description
NotSet
Sim
Fem
Ideal
Master
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.