AttributeGroupDescriptionCollection Class¶
-
class
NXOpen.PDM.
AttributeGroupDescriptionCollection
¶ Bases:
object
Represents a collection of attribute group description objects.
A smaller list of attribute groups descriptions can be retrieved by using the method
NXOpen.PDM.IAttributeGroupOwner.GetAttributeGroupDescriptions()
for classes that implement theNXOpen.PDM.IAttributeGroupOwner
interface. To obtain an instance of this class, refer toNXOpen.PDM.PdmSession
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.PDM.AttributeGroupDescription with the given identifier as recorded in a journal. |
Method Detail¶
FindObject¶
-
AttributeGroupDescriptionCollection.
FindObject
¶ Finds the
NXOpen.PDM.AttributeGroupDescription
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier to be found Returns: AttributeGroupDescription found, or null if no such attribute group description exists. Return type: NXOpen.PDM.AttributeGroupDescription
New in version NX9.0.0.
License requirements: None.