OptionType Enumeration¶
-
class
NXOpen.Options.
OptionType
¶ Bases:
object
Describes type of an option. Enum Members
Enum Member Enum Member Description Int Option value is an integer number Real Option value is a real number String Option value is an ascii string StringList Option value is a list of ascii strings Logical Option value is logical Utf8string Option value is a utf8 string Utf8stringList Option value is a list of utf8 strings ReorderSelList Option value is a list which can be selected and re-ordered -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-