DraftingStandardChangeList Class¶
-
class
NXOpen.Options.
DraftingStandardChangeList
¶ Bases:
NXOpen.TransientObject
Records changes to option values at the specified level.
A DraftingStandardChangeList is created with a given level, and all of the edit operations apply to that level for drafting standard defaults. Each method for setting a value throws an error if the option value is locked at a higher level, or the specified value is not valid.
All methods in this class use an option name as a unique identifier for accessing individual options and throw an error if an option with the given name is not found. All existing option names and their allowed values are described in the Online Documentation.
Use
Options.OptionsManager.NewOptionsDraftingStandardChangeList()
to create a new instance of this classNew in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CurrentLevel | Returns the current level of options |
Methods¶
Method | Description |
---|---|
Dispose | Dispose the changes |
Load | Load the drafting standard defaults at the current level. |
LockValue | Lock option value. |
Save | Saves the drafting standard defaults at the current level. |
SetUserComment | Sets the user comment. |
SetUtf8Value | Sets the value of a :py:class:` OptionsOptionType.Utf8string < OptionsOptionType>` option. |
SetValue | Sets the value of an :py:class:` OptionsOptionType.Int < OptionsOptionType>` option. |
SetValueOrder | Sets the value of a :py:class:` OptionsOptionType.ReorderSelList < OptionsOptionType>` option for which the list entries can be reordered. |
SetValueSelection | Sets the value of a :py:class:` OptionsOptionType.ReorderSelList < OptionsOptionType>` option for which the list entries can be reordered as well as selected. |
UnlockValue | Unlock option value. |
Property Detail¶
CurrentLevel¶
-
DraftingStandardChangeList.
CurrentLevel
¶ Returns the current level of options
-------------------------------------
Getter Method
Signature
CurrentLevel
Returns: Return type: NXOpen.Options.LevelType
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
DraftingStandardChangeList.
Dispose
¶ Dispose the changes
Signature
Dispose()
New in version NX5.0.0.
License requirements: None.
Load¶
-
DraftingStandardChangeList.
Load
¶ Load the drafting standard defaults at the current level.
Signature
Load()
New in version NX5.0.0.
License requirements: None.
LockValue¶
-
DraftingStandardChangeList.
LockValue
¶ Lock option value.
Signature
LockValue(name)
Parameters: name (str) – Option name New in version NX5.0.0.
License requirements: None.
Save¶
-
DraftingStandardChangeList.
Save
¶ Saves the drafting standard defaults at the current level.
Signature
Save()
New in version NX5.0.0.
License requirements: None.
SetUserComment¶
-
DraftingStandardChangeList.
SetUserComment
¶ Sets the user comment.
Throws an error if the value does not exist at this level.
Signature
SetUserComment(name, comment)
Parameters: - name (str) – Option name.
- comment (str) – User comment text.
New in version NX5.0.0.
License requirements: None.
SetUtf8Value¶
-
DraftingStandardChangeList.
SetUtf8Value
¶ Sets the value of a :py:class:` OptionsOptionType.Utf8string < OptionsOptionType>` option.
Throws an error if the option type is not :py:class:` OptionsOptionType.Utf8string < OptionsOptionType>`.
Signature
SetUtf8Value(name, value)
Parameters: - name (str) – Option name.
- value (str) – Option value
New in version NX6.0.0.
License requirements: None.
SetValue¶
-
DraftingStandardChangeList.
SetValue
¶ Overloaded method SetValue
SetValue(name, value)
SetValue(name, value)
SetValue(name, value)
SetValue(name, value)
SetValue(name, value)
-------------------------------------
Sets the value of an :py:class:` OptionsOptionType.Int < OptionsOptionType>` option. If the option is of type :py:class:` OptionsOptionType.Real < OptionsOptionType>` then the value parameter is converted to double. Throws an error if the option type is not :py:class:` OptionsOptionType.Int < OptionsOptionType>` or :py:class:` OptionsOptionType.Real < OptionsOptionType>`.
Signature
SetValue(name, value)
Parameters: - name (str) – Option name.
- value (int) – Option value.
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Sets the value of a :py:class:` OptionsOptionType.Real < OptionsOptionType>` option. Throws an error if the option type is not :py:class:` OptionsOptionType.Real < OptionsOptionType>`.
Signature
SetValue(name, value)
Parameters: - name (str) – Option name.
- value (float) – Option value.
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Sets the value of a :py:class:` OptionsOptionType.String < OptionsOptionType>` option. Throws an error if the option type is not :py:class:` OptionsOptionType.String < OptionsOptionType>`.
Signature
SetValue(name, value)
Parameters: - name (str) – Option name.
- value (str) – Option value
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Sets the value of a :py:class:` OptionsOptionType.StringList < OptionsOptionType>` option. Throws an error if the option type is not :py:class:` OptionsOptionType.StringList < OptionsOptionType>`.
Signature
SetValue(name, value)
Parameters: - name (str) – Option name.
- value (list of str) –
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Sets the value of a :py:class:` OptionsOptionType.Logical < OptionsOptionType>` option. Throws an error if the option type is not :py:class:` OptionsOptionType.Logical < OptionsOptionType>`.
Signature
SetValue(name, value)
Parameters: - name (str) – Option name.
- value (bool) – Option value
New in version NX5.0.0.
License requirements: None.
-------------------------------------
SetValueOrder¶
-
DraftingStandardChangeList.
SetValueOrder
¶ Sets the value of a :py:class:` OptionsOptionType.ReorderSelList < OptionsOptionType>` option for which the list entries can be reordered.
Throws an error if the option type is not :py:class:` OptionsOptionType.ReorderSelList < OptionsOptionType>`.
Signature
SetValueOrder(name, value)
Parameters: - name (str) – Option name.
- value (list of str) –
New in version NX7.5.0.
License requirements: None.
SetValueSelection¶
-
DraftingStandardChangeList.
SetValueSelection
¶ Sets the value of a :py:class:` OptionsOptionType.ReorderSelList < OptionsOptionType>` option for which the list entries can be reordered as well as selected.
Throws an error if the option type is not :py:class:` OptionsOptionType.ReorderSelList < OptionsOptionType>`.
Signature
SetValueSelection(name, selection, value)
Parameters: - name (str) – Option name.
- selection (list of bool) – the selection bit
- value (list of str) –
New in version NX7.5.0.
License requirements: None.