OptimizationBuilderOptimizationTargetType Enumeration¶
NXOpen.Optimization.OptimizationBuilder.OptimizationTargetType is an alias for NXOpen.Optimization.OptimizationBuilderOptimizationTargetType
-
class
NXOpen.Optimization.
OptimizationBuilderOptimizationTargetType
¶ Bases:
object
Optimization type for objective
Enum Members
Enum Member Enum Member Description Minimum Target is minimum value of design objective Maximum Target is maximum value of design objective Target Target is specified value of design objective -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-