OptimizationBuilderOptimizationConvergenceSpeedType Enumeration¶
NXOpen.Optimization.OptimizationBuilder.OptimizationConvergenceSpeedType is an alias for NXOpen.Optimization.OptimizationBuilderOptimizationConvergenceSpeedType
-
class
NXOpen.Optimization.
OptimizationBuilderOptimizationConvergenceSpeedType
¶ Bases:
object
Convergence speed type
Enum Members
Enum Member Enum Member Description Slow Slow convergence speed Medium Medium convergence speed Fast Fast convergence speed Infinite Infinite convergence speed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-