ObjectListDeleteOption Enumeration¶
NXOpen.ObjectList.DeleteOption is an alias for NXOpen.ObjectListDeleteOption
-
class
NXOpen.
ObjectListDeleteOption
¶ Bases:
object
Used to indicate whether to delete the object when removing it from the list
Enum Members
Enum Member Enum Member Description Delete Delete the object NoDelete Remove the object without deleting it -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-