OMAttribute Class¶
-
class
NXOpen.
OMAttribute
¶ Bases:
NXOpen.TaggedObject
,NXOpen.IOMName
Represents a OMAttribute.
This is for internal testing only.
This class is for internal testing only.
New in version NX3.0.0.
Methods¶
Method | Description |
---|---|
CompareWith | Compare with |
GetInfo | Returns the info |
GetObjectName | Returns the object name |
Enumerations¶
OMAttributeType Enumeration | For internal testing |
Structs¶
OMAttributeInfo_Struct Struct | For internal testing |
Method Detail¶
CompareWith¶
-
OMAttribute.
CompareWith
¶ Compare with
Signature
CompareWith(other)
Parameters: other ( NXOpen.IOMName
) –Returns: Return type: bool New in version NX3.0.0.
License requirements: None.
GetInfo¶
-
OMAttribute.
GetInfo
¶ Returns the info
Signature
GetInfo()
Returns: Return type: NXOpen.OMAttributeInfo_Struct
New in version NX3.0.0.
License requirements: None.