MovieSettingsBuilderCaptureAreaChoices Enumeration¶
NXOpen.MovieSettingsBuilder.CaptureAreaChoices is an alias for NXOpen.MovieSettingsBuilderCaptureAreaChoices
-
class
NXOpen.
MovieSettingsBuilderCaptureAreaChoices
¶ Bases:
object
Indicates the are being recorded in the movie.
Enum Members
Enum Member Enum Member Description Graphics Specifies that the NX graphics contents are to be recorded NxWindow Specifies that the NX window contents are to be recorded Desktop Specifies that the Desktop contents are to be recorded -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-