VectorForceCollection Class¶
-
class
NXOpen.Motion.
VectorForceCollection
¶ Bases:
object
Represents a collection of vector force objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX5.0.0.
Methods¶
Method | Description |
---|---|
CreateVectorForceBuilder | Creates a NXOpen.Motion.JointDriverBuilder |
FindObject | Finds the NXOpen.Motion.VectorForce with the given name. |
Method Detail¶
CreateVectorForceBuilder¶
-
VectorForceCollection.
CreateVectorForceBuilder
¶ Creates a
NXOpen.Motion.JointDriverBuilder
Signature
CreateVectorForceBuilder(vectorforce)
Parameters: vectorforce ( NXOpen.Motion.VectorForce
) – “NXOpen.Motion.VectorForce
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.VectorForceBuilder
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
VectorForceCollection.
FindObject
¶ Finds the
NXOpen.Motion.VectorForce
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.VectorForce
.Returns: NXOpen.Motion.VectorForce
with this name.Return type: NXOpen.Motion.VectorForce
New in version NX5.0.0.
License requirements: mechanisms (“MECHANISMS”)