UserDefinedSectionBuilder Class¶
-
class
NXOpen.Motion.
UserDefinedSectionBuilder
¶ Bases:
NXOpen.Motion.BaseSectionBuilder
Represents a
Motion.UserDefinedSectionBuilder
.To create a new instance of this class, use
NXOpen.Motion.BaseSectionCollection.CreateUserDefinedSectionBuilder()
New in version NX12.0.0.
Properties¶
Property | Description |
---|---|
Area | Returns the area |
DisplayScale | Returns or sets the icon display scale |
GroupName | Returns or sets the group name |
GroupType | Returns or sets the group type |
InertiaIyy | Returns the inertia Iyy |
InertiaIzy | Returns the inertia Izy |
InertiaIzz | Returns the inertia Izz |
InertiaJ | Returns the inertia J |
Name | Returns or sets the name of the base section object |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Area¶
-
UserDefinedSectionBuilder.
Area
¶ Returns the area
-------------------------------------
Getter Method
Signature
Area
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
InertiaIyy¶
-
UserDefinedSectionBuilder.
InertiaIyy
¶ Returns the inertia Iyy
-------------------------------------
Getter Method
Signature
InertiaIyy
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
InertiaIzy¶
-
UserDefinedSectionBuilder.
InertiaIzy
¶ Returns the inertia Izy
-------------------------------------
Getter Method
Signature
InertiaIzy
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
InertiaIzz¶
-
UserDefinedSectionBuilder.
InertiaIzz
¶ Returns the inertia Izz
-------------------------------------
Getter Method
Signature
InertiaIzz
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
InertiaJ¶
-
UserDefinedSectionBuilder.
InertiaJ
¶ Returns the inertia J
-------------------------------------
Getter Method
Signature
InertiaJ
Returns: Return type: NXOpen.Expression
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
Validate¶
-
UserDefinedSectionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.