TirePropertyFtCollection Class¶
-
class
NXOpen.Motion.
TirePropertyFtCollection
¶ Bases:
object
Represents a collection of Motion FTire Tire Property elements
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateTirePropertyFtBuilder | Return NXOpen.Motion.TirePropertyFtBuilder object |
FindObject | Finds the NXOpen.Motion.TirePropertyFt with the given name. |
Method Detail¶
CreateTirePropertyFtBuilder¶
-
TirePropertyFtCollection.
CreateTirePropertyFtBuilder
¶ Return
NXOpen.Motion.TirePropertyFtBuilder
objectSignature
CreateTirePropertyFtBuilder(tireProperty)
Parameters: tireProperty ( NXOpen.Motion.TirePropertyFt
) –NXOpen.Motion.TirePropertyFt
to be edited, if None then create a new oneReturns: TirePropertyFtBuilder object Return type: NXOpen.Motion.TirePropertyFtBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
TirePropertyFtCollection.
FindObject
¶ Finds the
NXOpen.Motion.TirePropertyFt
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.TirePropertyFt
Returns: NXOpen.Motion.TirePropertyFt
with this nameReturn type: NXOpen.Motion.TirePropertyFt
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)