AmbientTempFunction |
Returns or sets the ambient temperature function |
AmbientTempProfile |
Returns the Profile for Ambient Temperature. |
AmbientTempTypeSelection |
Returns or sets the ambient temperature type. |
AmbientTempValue |
Returns the ambient temperature constant value. |
ContactKinematics |
Returns or sets the Contact Kinematics (Effective Rolling Radius, Slip Velocities, Surface Normal). |
ContactLengthWidth |
Returns or sets the contact length/width. |
ContactPointGlobal |
Returns or sets the contact point surface friction global. |
ContactPointRoadRef |
Returns or sets the contact point surface friction road frame. |
CorrectorIter |
Returns the corrector iterations. |
DisplayScale |
Returns or sets the icon display scale |
EnergyLoss |
Returns or sets the wear indicator. |
EnergyLossOfSpecificEntities |
Returns or sets the Energy Loss Of Specific Entities. |
EnergyLossPerSegment |
Returns or sets the Energy Loss Per Cross Section Segment Activates specific CDTire results: eloss_gl, eloss_01 . |
GroupName |
Returns or sets the group name |
GroupType |
Returns or sets the group type |
Inclination |
Returns or sets the inclination and slip angle, slip loaded radius, rim rotation. |
InflationPressureFunction |
Returns or sets the inflation pressure function |
InflationPressureProfile |
Returns the Profile for Inflation Pressure. |
InflationPressureTypeSelection |
Returns or sets the inflation pressure type. |
InflationPressureValue |
Returns the inflation pressure constant value. |
ModelTypeSelection |
Returns or sets the CDTire model type. |
Name |
Returns or sets the name of the Tire Property |
PrimaryParamFile |
Returns or sets the primary parameter file. |
RimRoadGlobal |
Returns or sets the rim road global frame. |
RimRoadTydexW |
Returns or sets the rim road tydex-W frame. |
RimTydexCH |
Returns or sets the rim Tydex-C and Tydex-H frames. |
RoadGlobal |
Returns or sets the road center global. |
SolverResults |
Returns or sets the solver results Activates specific CDTire results: Integration step size (h);Time integration error (err); |
StaticHold |
Returns or sets the static hold. |
StaticRadius |
Returns the static radius. |
StaticVerticalStiffness |
Returns the static vertical stiffness. |
Tag |
Returns the Tag for this object. |
TimeStatistics |
Returns or sets the time statistics Activates specific CDTire results: Simulation time (time); CDTire tire model type (submodel); CDTire road model type (type); CPU time for this tire (cpu_time); |
TireControlFile |
Returns or sets the tire control file. |
WearIndicatorPerSegment |
Returns or sets the Wear Indicator Per Cross Section Segment. |
WheelGlobal |
Returns or sets the wheel center global. |
WheelRoadRef |
Returns or sets the wheel center road reference frame. |