TirePropertyBasicParametersCorneringType Enumeration¶
NXOpen.Motion.TirePropertyBasicParameters.CorneringType is an alias for NXOpen.Motion.TirePropertyBasicParametersCorneringType
-
class
NXOpen.Motion.
TirePropertyBasicParametersCorneringType
¶ Bases:
object
A constant will be used for the Cornering Stiffness when CorneringType is ‘Cornering’. When CorneringType is ‘Carpet’, a surface will be used from a data table file.
Enum Members
Enum Member Enum Member Description Cornering Carpet -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-