TirePropertyAdvancedParametersContactType Enumeration¶
NXOpen.Motion.TirePropertyAdvancedParameters.ContactType is an alias for NXOpen.Motion.TirePropertyAdvancedParametersContactType
-
class
NXOpen.Motion.
TirePropertyAdvancedParametersContactType
¶ Bases:
object
The block type can be Function when a spline curve is used or Profile when a profile is used.
Enum Members
Enum Member Enum Member Description Function Profile -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-