TireBuilderType Enumeration¶
NXOpen.Motion.TireBuilder.Type is an alias for NXOpen.Motion.TireBuilderType
-
class
NXOpen.Motion.
TireBuilderType
¶ Bases:
object
the Tire type. Each tire type has a specific tire property associated. A tire is invalid without a tire property associated.
Enum Members
Enum Member Enum Member Description Basic for Basic Tire Model Tno for TNO Tire Model CDTire for CDTire Tire Model FTire for FTire Tire Model Motorcycle for Motorcycle Tire Model NonInertial for Non-Inertial Tire Model -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-