TextBasedElementBuilderTypeChoices Enumeration¶
NXOpen.Motion.TextBasedElementBuilder.TypeChoices is an alias for NXOpen.Motion.TextBasedElementBuilderTypeChoices
-
class
NXOpen.Motion.
TextBasedElementBuilderTypeChoices
¶ Bases:
object
the text based element type - multiple values
Enum Members
Enum Member Enum Member Description ThreePointForce ThreePointTorque AllKinematicDirectionSensor AllForceDirectionSensor AeroAeroForce AeroHydroForce AeroVehicleForce CustomizedSolver StiTire StiTireProperty BumpStopContact SphereToGroundContact GearContact ThreeLinkSuspension FourLinkSuspension FiveLinkSuspension RollIaxSuspension SteerIaxSuspension HotchKissSuspension McPhersonSuspension DoubleAArmSuspension PivotBeamSuspension Vehicle SpeedSweep SystemProperty DynamicProperty KinematicProperty StaticProperty PreloadProperty InverseProperty LinearizationProperty RestartProperty AdvancedSolution Gear Generic Fmi PointToPointConstraint OrientationConstraint FunctioncurveControlInput PathFollowerControlInput UserDefinedControlInput SpecialControlInput LinearControlOutput MassPropertyControlOutput LinkInitialCondition ScrewJointOrSpringInitialCondition FlexibleLinkInitialCondition TireInitialCondition StaticVehicleAlignment SprungMass UserDefinedForce GlobalDirectionsLinkDriver DotOneLinkDriver DotTwoLinkDriver CurveOnCurveConstraintDriver FixedJointDriver LinkCouplerDriver -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-