SubmechanismPositionerCollection Class¶
-
class
NXOpen.Motion.
SubmechanismPositionerCollection
¶ Bases:
object
Represents a collection of Submechanmism Positioner objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreatePositionerBuilder | Creates a NXOpen.Motion.SubmechanismPositionerBuilder |
FindObject | Finds the NXOpen.Motion.SubmechanismPositioner object with the given name. |
Method Detail¶
CreatePositionerBuilder¶
-
SubmechanismPositionerCollection.
CreatePositionerBuilder
¶ Creates a
NXOpen.Motion.SubmechanismPositionerBuilder
Signature
CreatePositionerBuilder(positioner)
Parameters: positioner ( NXOpen.Motion.SubmechanismPositioner
) –NXOpen.Motion.SubmechanismPositioner
to be editedReturns: SubmechanismPositionerBuilder object Return type: NXOpen.Motion.SubmechanismPositionerBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
SubmechanismPositionerCollection.
FindObject
¶ Finds the
NXOpen.Motion.SubmechanismPositioner
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.SubmechanismPositioner
.Returns: NXOpen.Motion.SubmechanismPositioner
with this name.Return type: NXOpen.Motion.SubmechanismPositioner
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)