StandardSectionBuilderStandardSectionType Enumeration¶
NXOpen.Motion.StandardSectionBuilder.StandardSectionType is an alias for NXOpen.Motion.StandardSectionBuilderStandardSectionType
-
class
NXOpen.Motion.
StandardSectionBuilderStandardSectionType
¶ Bases:
object
the standard section type
Enum Members
Enum Member Enum Member Description Rod Rod Tube Tube Bar Bar Box Box Box1 Box1 I I I1 I1 T T T1 T1 T2 T2 Chan Chan Chan1 Chan1 Chan2 Chan2 Hat Hat Hat1 Hat1 H H L L Z Z Hexa Hexa Cross Cross -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-