SplineBeamPropertyCollection Class¶
-
class
NXOpen.Motion.
SplineBeamPropertyCollection
¶ Bases:
object
Represents a collection of SplineBeamProperty
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateSplineBeamPropertyBuilder | Creates a Motion.SplineBeamPropertyBuilder |
FindObject | Finds the NXOpen.Motion.SplineBeamProperty with the given name. |
Method Detail¶
CreateSplineBeamPropertyBuilder¶
-
SplineBeamPropertyCollection.
CreateSplineBeamPropertyBuilder
¶ Creates a
Motion.SplineBeamPropertyBuilder
Signature
CreateSplineBeamPropertyBuilder(splineBeamProperty)
Parameters: splineBeamProperty ( NXOpen.Motion.SplineBeamProperty
) –NXOpen.Motion.SplineBeamProperty
to be edited, if None then create a new oneReturns: SplineBeamPropertyBuilder object Return type: NXOpen.Motion.SplineBeamPropertyBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
SplineBeamPropertyCollection.
FindObject
¶ Finds the
NXOpen.Motion.SplineBeamProperty
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.SplineBeamProperty
Returns: NXOpen.Motion.SplineBeamProperty
with this nameReturn type: NXOpen.Motion.SplineBeamProperty
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)