SplineBeamCollection Class¶
-
class
NXOpen.Motion.
SplineBeamCollection
¶ Bases:
object
Represents a collection of SplineBeams
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateSplineBeamBuilder | Creates a Motion.SplineBeamBuilder |
FindObject | Finds the NXOpen.Motion.SplineBeam with the given name. |
Method Detail¶
CreateSplineBeamBuilder¶
-
SplineBeamCollection.
CreateSplineBeamBuilder
¶ Creates a
Motion.SplineBeamBuilder
Signature
CreateSplineBeamBuilder(splineBeam)
Parameters: splineBeam ( NXOpen.Motion.SplineBeam
) –NXOpen.Motion.SplineBeam
to be edited, if None then create a new oneReturns: SplineBeamBuilder object Return type: NXOpen.Motion.SplineBeamBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
SplineBeamCollection.
FindObject
¶ Finds the
NXOpen.Motion.SplineBeam
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.SplineBeam
Returns: NXOpen.Motion.SplineBeam
with this nameReturn type: NXOpen.Motion.SplineBeam
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)