SplineBeamBuilderDefinitionMethodType Enumeration¶
NXOpen.Motion.SplineBeamBuilder.DefinitionMethodType is an alias for NXOpen.Motion.SplineBeamBuilderDefinitionMethodType
-
class
NXOpen.Motion.
SplineBeamBuilderDefinitionMethodType
¶ Bases:
object
the definition method type
Enum Members
Enum Member Enum Member Description Manual Manual Curve Curve -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-