SegmentCollection Class¶
-
class
NXOpen.Motion.
SegmentCollection
¶ Bases:
object
Represents a collection of Segment objects, only creation is supported
To obtain an instance of this class, refer to
NXOpen.Motion.Road
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Motion.Segment object with the given name. |
Method Detail¶
FindObject¶
-
SegmentCollection.
FindObject
¶ Finds the
NXOpen.Motion.Segment
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Name of the Segment object. Returns: NXOpen.Motion.Segment
object with this name.Return type: NXOpen.Motion.Segment
New in version NX11.0.0.
License requirements: None.