SegmentBuilderTypeChoices Enumeration¶
NXOpen.Motion.SegmentBuilder.TypeChoices is an alias for NXOpen.Motion.SegmentBuilderTypeChoices
-
class
NXOpen.Motion.
SegmentBuilderTypeChoices
¶ Bases:
object
type attribute of the segment
Enum Members
Enum Member Enum Member Description Straight Straight ConstantRadius Constant Radius LaneChange Lane Change Slalom Slalom UserDefined User Defined -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-