ScalarTorqueCollection Class¶
-
class
NXOpen.Motion.
ScalarTorqueCollection
¶ Bases:
object
Represents a collection of motion scalar torque
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateScalarTorqueBuilder | Return NXOpen.Motion.ScalarTorqueBuilder object |
FindObject | Finds the NXOpen.Motion.ScalarTorque with the given name. |
Method Detail¶
CreateScalarTorqueBuilder¶
-
ScalarTorqueCollection.
CreateScalarTorqueBuilder
¶ Return
NXOpen.Motion.ScalarTorqueBuilder
objectSignature
CreateScalarTorqueBuilder(scalarTorque)
Parameters: scalarTorque ( NXOpen.Motion.ScalarTorque
) –NXOpen.Motion.ScalarTorque
to be edited, if None then create a new oneReturns: ScalarTorqueBuilder object Return type: NXOpen.Motion.ScalarTorqueBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
ScalarTorqueCollection.
FindObject
¶ Finds the
NXOpen.Motion.ScalarTorque
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.ScalarTorque
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)