ScalarTorqueBuilderScalarTorqueType Enumeration¶
NXOpen.Motion.ScalarTorqueBuilder.ScalarTorqueType is an alias for NXOpen.Motion.ScalarTorqueBuilderScalarTorqueType
-
class
NXOpen.Motion.
ScalarTorqueBuilderScalarTorqueType
¶ Bases:
object
the torque type
Enum Members
Enum Member Enum Member Description Joint Scalar Torque Type Joint. Requires a Joint as input. Link Scalar Torque Type Link. Requires an action and base link attachment. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-