ScalarForceCollection Class¶
-
class
NXOpen.Motion.
ScalarForceCollection
¶ Bases:
object
Represents a Scalar Force Collection.
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
CreateScalarForceBuilder | Return NXOpen.Motion.ScalarForceBuilder object |
FindObject | Finds the NXOpen.Motion.ScalarForce with the given name. |
Method Detail¶
CreateScalarForceBuilder¶
-
ScalarForceCollection.
CreateScalarForceBuilder
¶ Return
NXOpen.Motion.ScalarForceBuilder
objectSignature
CreateScalarForceBuilder(scalarForce)
Parameters: scalarForce ( NXOpen.Motion.ScalarForce
) –NXOpen.Motion.ScalarForce
to be edited, if None then create a new oneReturns: ScalarForceBuilder object Return type: NXOpen.Motion.ScalarForceBuilder
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
ScalarForceCollection.
FindObject
¶ Finds the
NXOpen.Motion.ScalarForce
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.ScalarForce
New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)