ScalarForceBuilderDirectionType Enumeration¶
NXOpen.Motion.ScalarForceBuilder.DirectionType is an alias for NXOpen.Motion.ScalarForceBuilderDirectionType
-
class
NXOpen.Motion.
ScalarForceBuilderDirectionType
¶ Bases:
object
the Direction type. Each direction type has a specific direction associated. A Scalar Force is invalid without a direction associated.
Enum Members
Enum Member Enum Member Description Translational for Translational direction X for X direction Y for Y dircetion Z for Z direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-