ScalarForceBuilderApplicationType Enumeration¶
NXOpen.Motion.ScalarForceBuilder.ApplicationType is an alias for NXOpen.Motion.ScalarForceBuilderApplicationType
-
class
NXOpen.Motion.
ScalarForceBuilderApplicationType
¶ Bases:
object
the application type. Each application type has a specific application associated. A Scalar Force is invalid without the type of application
Enum Members
Enum Member Enum Member Description ActionReaction for Action-Reaction Appplication type ActionOnly for Action Only Appplication type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-