RoadBuilderSurfaceDatatypeChoices Enumeration¶
NXOpen.Motion.RoadBuilder.SurfaceDatatypeChoices is an alias for NXOpen.Motion.RoadBuilderSurfaceDatatypeChoices
-
class
NXOpen.Motion.
RoadBuilderSurfaceDatatypeChoices
¶ Bases:
object
data type attribute of the surface data
Enum Members
Enum Member Enum Member Description SplineCurve Function SplineSurface Spline Surface defined by 3D Profile Rsm1000 RSM1000 Rsm1002 RSM1002 Rsm2000 RSM2000 Rsm3000 RSM3000 OpenCRG OpenCRG RoadDataFile Road Data File Profile2D Profile 2D -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-