ResultMeasureBuilder Class¶
-
class
NXOpen.Motion.
ResultMeasureBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Motion.ResultMeasure
builderTo create a new instance of this class, use
NXOpen.Motion.ResultMeasureCollection.CreateResultMeasureBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
ExpName | Returns or sets the expression name |
InterferenceType | Returns or sets the interference result type |
ReferenceObject | Returns the reference object |
ResultType | Returns or sets the result type |
Solution | Returns or sets the solution |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitResultMeasure | Commits the Builder, and returns the created result measure object. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
ExpName¶
-
ResultMeasureBuilder.
ExpName
¶ Returns or sets the expression name
-------------------------------------
Getter Method
Signature
ExpName
Returns: Return type: str New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ExpName
Parameters: name (str) – New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
InterferenceType¶
-
ResultMeasureBuilder.
InterferenceType
¶ Returns or sets the interference result type
-------------------------------------
Getter Method
Signature
InterferenceType
Returns: Return type: NXOpen.Motion.ResultMeasureInterferenceType
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
InterferenceType
Parameters: interferenceType ( NXOpen.Motion.ResultMeasureInterferenceType
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
ReferenceObject¶
-
ResultMeasureBuilder.
ReferenceObject
¶ Returns the reference object
-------------------------------------
Getter Method
Signature
ReferenceObject
Returns: Return type: NXOpen.SelectNXObject
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
ResultType¶
-
ResultMeasureBuilder.
ResultType
¶ Returns or sets the result type
-------------------------------------
Getter Method
Signature
ResultType
Returns: Return type: NXOpen.Motion.ResultMeasureResultType
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
ResultType
Parameters: resultType ( NXOpen.Motion.ResultMeasureResultType
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Solution¶
-
ResultMeasureBuilder.
Solution
¶ Returns or sets the solution
-------------------------------------
Getter Method
Signature
Solution
Returns: Return type: NXOpen.Motion.MotionSolution
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
-------------------------------------
Setter Method
Signature
Solution
Parameters: solution ( NXOpen.Motion.MotionSolution
) –New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Method Detail¶
CommitResultMeasure¶
-
ResultMeasureBuilder.
CommitResultMeasure
¶ Commits the Builder, and returns the created result measure object.
Signature
CommitResultMeasure()
Returns: Return type: NXOpen.TaggedObject
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
Validate¶
-
ResultMeasureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.