PostProcessEnvelopeTolerance_Struct Struct¶
NXOpen.Motion.PostProcess.EnvelopeTolerance is an alias for NXOpen.Motion.PostProcessEnvelopeTolerance_Struct
-
class
NXOpen.Motion.
PostProcessEnvelopeTolerance_Struct
¶ Bases:
object
Contains settings for envelope tolerance .
Constructor: NXOpen.Motion.PostProcess.EnvelopeTolerance()
Fields¶
Field | Description |
---|---|
AccuracyMode | Accuracy mode. |
ToleranceType | Indicates if envelopeTolerance is specified as percentage value or absolute value. |
Tolerance | Tolerance value. |
DecimationEnabled | Indicates if decimation is enabled or not. |
DecimationFactor | Specifies targeted decimation rate which is decimated body/original body. |
DecimationMaxError | Specifies max decimation error: (bigger than 0): percentage, (less than 0): absolute value. |
AccuracyMode¶
-
PostProcessEnvelopeTolerance_Struct.
AccuracyMode
¶ Accuracy mode.
Motion.PostProcessEnvelopeAccuracyModes
.-------------------------------------
Field Value Type:
NXOpen.Motion.PostProcessEnvelopeAccuracyModes
ToleranceType¶
-
PostProcessEnvelopeTolerance_Struct.
ToleranceType
¶ Indicates if envelopeTolerance is specified as percentage value or absolute value.
Used only if accurcayMode is
Motion.PostProcessEnvelopeAccuracyModes.Custom
.-------------------------------------
Field Value Type:
NXOpen.Motion.PostProcessEnvelopeToleranceTypes
Tolerance¶
-
PostProcessEnvelopeTolerance_Struct.
Tolerance
¶ Tolerance value.
Used only if accurcayMode is
Motion.PostProcessEnvelopeAccuracyModes.Custom
.-------------------------------------
Field Value Type:float
DecimationEnabled¶
-
PostProcessEnvelopeTolerance_Struct.
DecimationEnabled
¶ Indicates if decimation is enabled or not.
Used only if accurcayMode is
Motion.PostProcessEnvelopeAccuracyModes.Custom
.-------------------------------------
Field Value Type:bool
DecimationFactor¶
-
PostProcessEnvelopeTolerance_Struct.
DecimationFactor
¶ Specifies targeted decimation rate which is decimated body/original body.
Used only if accurcayMode is
Motion.PostProcessEnvelopeAccuracyModes.Custom
.-------------------------------------
Field Value Type:float
DecimationMaxError¶
-
PostProcessEnvelopeTolerance_Struct.
DecimationMaxError
¶ Specifies max decimation error: (bigger than 0): percentage, (less than 0): absolute value.
Used only if accurcayMode is
Motion.PostProcessEnvelopeAccuracyModes.Custom
.-------------------------------------
Field Value Type:float