PackagingMeasureBuilderMeasureType Enumeration¶
NXOpen.Motion.PackagingMeasureBuilder.MeasureType is an alias for NXOpen.Motion.PackagingMeasureBuilderMeasureType
-
class
NXOpen.Motion.
PackagingMeasureBuilderMeasureType
¶ Bases:
object
Measure type
Enum Members
Enum Member Enum Member Description MinimumDistance Measure minimum distance between objects. Angle Measure angle between lines or linear edges. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-