PackagingMeasureBuilderMeasureCondition Enumeration¶
NXOpen.Motion.PackagingMeasureBuilder.MeasureCondition is an alias for NXOpen.Motion.PackagingMeasureBuilderMeasureCondition
-
class
NXOpen.Motion.
PackagingMeasureBuilderMeasureCondition
¶ Bases:
object
Measure condition
Enum Members
Enum Member Enum Member Description LessThan Stop event defined by minimum measurement less than threshold value. GreaterThan Stop event defined by minimum measurement greater than threshold value. EqualTo Stop event defined by minimum measurement equal to threshold (target) value. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-