PackagingInterferenceBuilderMode Enumeration¶
NXOpen.Motion.PackagingInterferenceBuilder.Mode is an alias for NXOpen.Motion.PackagingInterferenceBuilderMode
-
class
NXOpen.Motion.
PackagingInterferenceBuilderMode
¶ Bases:
object
Interference calculation mode type
Enum Members
Enum Member Enum Member Description Faceted Interference calculated by Faceted method. Faceted is only allowed for action type of :py:class:` NXOpen.Motion.PackagingInterferenceBuilderAction.CreateSolids < NXOpen.Motion.PackagingInterferenceBuilderAction>`. PreciseSolid Interference calculated by Precise Solid method. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-