PackagingInterferenceBuilderFrame Enumeration¶
NXOpen.Motion.PackagingInterferenceBuilder.Frame is an alias for NXOpen.Motion.PackagingInterferenceBuilderFrame
-
class
NXOpen.Motion.
PackagingInterferenceBuilderFrame
¶ Bases:
object
Interference solid reference frame type. Only used for action type of :py:class:` NXOpen.Motion.PackagingInterferenceBuilderAction.CreateSolids < NXOpen.Motion.PackagingInterferenceBuilderAction>`.
Enum Members
Enum Member Enum Member Description Absolute Interference solids positioned in absolute coordinate system. FirstSet Interference solids positioned relative to interfering links in first set. SecondSet Interference solids positioned relative to interfering links in second set. BothSets Interference solids positioned relative to interfering links in both sets. Selected Interference solids positioned relative to user selected links. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-