PackagingCollection Class¶
-
class
NXOpen.Motion.
PackagingCollection
¶ Bases:
object
Represents a collection of Packaging objects
To obtain an instance of this class, refer to
NXOpen.Part
New in version NX4.0.0.
Methods¶
Method | Description |
---|---|
CreateInterferenceBuilder | Creates an NXOpen.Motion.PackagingInterferenceBuilder . |
CreateMeasureBuilder | Creates a NXOpen.Motion.PackagingMeasureBuilder . |
CreateTraceBuilder | Creates a NXOpen.Motion.PackagingTraceBuilder . |
FindObject | Finds the NXOpen.Motion.Packaging object with the given name. |
Method Detail¶
CreateInterferenceBuilder¶
-
PackagingCollection.
CreateInterferenceBuilder
¶ Creates an
NXOpen.Motion.PackagingInterferenceBuilder
.This class is used to construct an
NXOpen.Motion.PackagingInterference
object.Signature
CreateInterferenceBuilder(interference)
Parameters: interference ( NXOpen.Motion.PackagingInterference
) –NXOpen.Motion.PackagingInterference
object to edit. None indicates that a newNXOpen.Motion.PackagingInterference
object is being created.Returns: NXOpen.Motion.PackagingInterferenceBuilder
objectReturn type: NXOpen.Motion.PackagingInterferenceBuilder
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
CreateMeasureBuilder¶
-
PackagingCollection.
CreateMeasureBuilder
¶ Creates a
NXOpen.Motion.PackagingMeasureBuilder
.This class is used to construct a
NXOpen.Measure
object.Signature
CreateMeasureBuilder(measure)
Parameters: measure ( NXOpen.Motion.PackagingMeasure
) –NXOpen.Measure
object to edit. None indicates that a newNXOpen.Measure
object is being created.Returns: NXOpen.Motion.PackagingMeasureBuilder
objectReturn type: NXOpen.Motion.PackagingMeasureBuilder
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
CreateTraceBuilder¶
-
PackagingCollection.
CreateTraceBuilder
¶ Creates a
NXOpen.Motion.PackagingTraceBuilder
.This class is used to construct a
NXOpen.Motion.PackagingTrace
object.Signature
CreateTraceBuilder(trace)
Parameters: trace ( NXOpen.Motion.PackagingTrace
) –NXOpen.Motion.PackagingTrace
object to edit. None indicates that a newNXOpen.Motion.PackagingTrace
object is being created.Returns: NXOpen.Motion.PackagingTraceBuilder
objectReturn type: NXOpen.Motion.PackagingTraceBuilder
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
PackagingCollection.
FindObject
¶ Finds the
NXOpen.Motion.Packaging
object with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Name of the Packaging object. Returns: NXOpen.Motion.Packaging
object with this name.Return type: NXOpen.Motion.Packaging
New in version NX4.0.0.
License requirements: mechanisms (“MECHANISMS”)