MotionEnvironmentJointWizardStatus Enumeration¶
NXOpen.Motion.MotionEnvironment.JointWizardStatus is an alias for NXOpen.Motion.MotionEnvironmentJointWizardStatus
-
class
NXOpen.Motion.
MotionEnvironmentJointWizardStatus
¶ Bases:
object
Represents the on-off status of joint wizard
Enum Members
Enum Member Enum Member Description Undefined Undefined status Off Joint Wizard is turned off On Joint Wizard is turned on -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-