MechatronicsPortCollection Class¶
-
class
NXOpen.Motion.
MechatronicsPortCollection
¶ Bases:
object
Represents a collection of ports used as outputs by Mechatronics
To obtain an instance of this class, refer to
NXOpen.Motion.Mechatronics
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
FindObject | Finds the NXOpen.Motion.ControlPort variable with the given name. |
Method Detail¶
FindObject¶
-
MechatronicsPortCollection.
FindObject
¶ Finds the
NXOpen.Motion.ControlPort
variable with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.ControlPort
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)