MechatronicsCollection Class¶
-
class
NXOpen.Motion.
MechatronicsCollection
¶ Bases:
object
Represents a collection of Mechatronics
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX11.0.0.
Methods¶
Method | Description |
---|---|
CreateMechatronicsBuilder | Creates a Motion.MechatronicsBuilder |
FindObject | Finds the NXOpen.Motion.Mechatronics with the given name. |
Method Detail¶
CreateMechatronicsBuilder¶
-
MechatronicsCollection.
CreateMechatronicsBuilder
¶ Creates a
Motion.MechatronicsBuilder
Signature
CreateMechatronicsBuilder(mechatronics)
Parameters: mechatronics ( NXOpen.Motion.Mechatronics
) –Returns: Return type: NXOpen.Motion.MechatronicsBuilder
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
MechatronicsCollection.
FindObject
¶ Finds the
NXOpen.Motion.Mechatronics
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – Returns: Return type: NXOpen.Motion.Mechatronics
New in version NX11.0.0.
License requirements: mechanisms (“MECHANISMS”)