MechanismImportNamingRule Enumeration¶
NXOpen.Motion.MechanismImport.NamingRule is an alias for NXOpen.Motion.MechanismImportNamingRule
-
class
NXOpen.Motion.
MechanismImportNamingRule
¶ Bases:
object
Naming Rule type to modify imported object’s name
Enum Members
Enum Member Enum Member Description NotSet Keeps imported object’s name as is AddPrefix Adds a prefix string to imported object’s name AddSuffix Adds a suffix string to imported object’s name -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-