MechanismExportPositionOrientationFormat Enumeration¶
NXOpen.Motion.MechanismExport.PositionOrientationFormat is an alias for NXOpen.Motion.MechanismExportPositionOrientationFormat
-
class
NXOpen.Motion.
MechanismExportPositionOrientationFormat
¶ Bases:
object
Format to export the position and orientation data.
Enum Members
Enum Member Enum Member Description TransformationMatrix Origin and X, Y, Z vectors Pqr P, Q, R points BryantAngles Origin and Bryant angles EulerAngles Origin and Euler angles EulerParameters Origin and Euler parameters -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-