MarkerBuilder Class¶
-
class
NXOpen.Motion.
MarkerBuilder
¶ Bases:
NXOpen.Builder
Represents a builder of Marker
To create a new instance of this class, use
NXOpen.Motion.MarkerCollection.CreateMarkerBuilder()
Default values.
Property Value DisplayScale 1 New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Csys | Returns or sets the csys |
DisplayScale | Returns or sets the display scale |
Name | Returns or sets the name |
OriginPoint | Returns or sets the origin point |
SelectLink | Returns the select link |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Csys¶
-
MarkerBuilder.
Csys
¶ Returns or sets the csys
-------------------------------------
Getter Method
Signature
Csys
Returns: Return type: NXOpen.CoordinateSystem
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Csys
Parameters: csys ( NXOpen.CoordinateSystem
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
DisplayScale¶
-
MarkerBuilder.
DisplayScale
¶ Returns or sets the display scale
-------------------------------------
Getter Method
Signature
DisplayScale
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayScale
Parameters: displayScale (float) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
Name¶
-
MarkerBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name
Parameters: name (str) – New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
OriginPoint¶
-
MarkerBuilder.
OriginPoint
¶ Returns or sets the origin point
-------------------------------------
Getter Method
Signature
OriginPoint
Returns: Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
OriginPoint
Parameters: originPoint ( NXOpen.Point
) –New in version NX6.0.0.
License requirements: mechanisms (“MECHANISMS”)
SelectLink¶
-
MarkerBuilder.
SelectLink
¶ Returns the select link
-------------------------------------
Getter Method
Signature
SelectLink
Returns: Return type: NXOpen.SelectNXObject
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
MarkerBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.