LoadTransferCollection Class¶
-
class
NXOpen.Motion.
LoadTransferCollection
¶ Bases:
object
Represents a collection of load transfer objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CreateLoadTransferBuilder | Creates a NXOpen.Motion.LoadTransferBuilder . |
FindObject | Finds the NXOpen.Motion.LoadTransfer with the given name. |
Method Detail¶
CreateLoadTransferBuilder¶
-
LoadTransferCollection.
CreateLoadTransferBuilder
¶ Creates a
NXOpen.Motion.LoadTransferBuilder
.If active
NXOpen.Motion.MotionSolution
is not present, builder will not be created.Signature
CreateLoadTransferBuilder(loadTransfer)
Parameters: loadTransfer ( NXOpen.Motion.LoadTransfer
) –NXOpen.Motion.LoadTransfer
to be edited, if None then create a new oneReturns: Return type: NXOpen.Motion.LoadTransferBuilder
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
LoadTransferCollection.
FindObject
¶ Finds the
NXOpen.Motion.LoadTransfer
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.LoadTransfer
.Returns: NXOpen.Motion.LoadTransfer
with this name.Return type: NXOpen.Motion.LoadTransfer
New in version NX9.0.0.
License requirements: mechanisms (“MECHANISMS”)