LinkCouplerCollection Class¶
-
class
NXOpen.Motion.
LinkCouplerCollection
¶ Bases:
object
Represents a collection of LinkCoupler objects
To obtain an instance of this class, refer to
NXOpen.Motion.MotionManager
New in version NX12.0.0.
Methods¶
Method | Description |
---|---|
CreateLinkCouplerBuilder | Creates a NXOpen.Motion.LinkCouplerBuilder |
FindObject | Finds the NXOpen.Motion.LinkCoupler with the given name. |
Method Detail¶
CreateLinkCouplerBuilder¶
-
LinkCouplerCollection.
CreateLinkCouplerBuilder
¶ Creates a
NXOpen.Motion.LinkCouplerBuilder
Signature
CreateLinkCouplerBuilder(linkCoupler)
Parameters: linkCoupler ( NXOpen.Motion.LinkCoupler
) –Returns: Return type: NXOpen.Motion.LinkCouplerBuilder
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)
FindObject¶
-
LinkCouplerCollection.
FindObject
¶ Finds the
NXOpen.Motion.LinkCoupler
with the given name.An exception will be thrown if no object can be found with given name.
Signature
FindObject(name)
Parameters: name (str) – The name of the NXOpen.Motion.LinkCoupler
.Returns: NXOpen.Motion.LinkCoupler
with this name.Return type: NXOpen.Motion.LinkCoupler
New in version NX12.0.0.
License requirements: mechanisms (“MECHANISMS”)